AXIS#.HOME.PERRTHRESH
Description
AXIS#.HOME.PERRTHRES is the maximum value the absolute following error (AXIS#.PL.ERR ) needs to exceed to detect a mechanical stop.
AXIS#.HOME.PERRTHRES is only used when homing against a mechanical stop using AXIS#.HOME.MODE is 8, 9 or 10.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read/Write |
|
Units |
Rotary: counts, rad, deg, custom units, 16-bit counts See Position Units for details. |
|
Range |
Depends on units. See Position Range for details. |
|
Default Value |
180 deg |
|
Data Type |
Float |
|
See Also |
|
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Fieldbus Information
| Fieldbus |
Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO Mappable |
|---|---|---|---|---|---|---|---|---|
| EtherCAT |
AXIS1.HOME.PERRTHRESH | 0x5008 | 0x6 | DINT | - | Position | RW | False |
| AXIS2.HOME.PERRTHRESH | 0x5108 | 0x6 | DINT | - | Position | RW | False |
Related Topics
Homing